Issue in booting from SD card

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Issue in booting from SD card

2,712 Views
rineet_kv
Contributor II

Hi,

We are using IMX 6UL with boot device as SD card. Getting following error.

mmc_init: -110, time 1450

*** Warning - MMC init failed, using default environment

Same SD card is working with the EVK board. I have pasted the logs below.

U-Boot 2017.03-nxp/imx_v2017.03_4.9.11_1.0.0_ga+ga2fea67 (Aug 24 2018 - 12:43:48 +0530)

 

CPU:   Freescale i.MX6UL rev1.2 528 MHz (running at 396 MHz)

CPU:   Commercial temperature grade (0C to 95C) at 39C

Reset cause: POR

Model: Freescale i.MX6 UltraLite 14x14 EVK Board

Board: MX6UL 14x14 EVK

DRAM:  512 MiB

MMC:   FSL_SDHC: 0, FSL_SDHC: 1

mmc_init: -110, time 1450

*** Warning - MMC init failed, using default environment

 

Display: TFT43AB (480x272)

Video: 480x272x24

In:    serial

Out:   serial

Err:   serial

mmc_init: -110, time 1450

Net:   No ethernet found.

Normal Boot

Hit any key to stop autoboot:  0

mmc_init: -110, time 1450

mmc_init: -110, time 1450

MMC: no card present

mmc_init: -123, time 2

Booting from net ...

No ethernet found.

No ethernet found.

Bad Linux ARM zImage magic!

Regards,

Rineet

Labels (1)
2 Replies

2,381 Views
igorpadykov
NXP Employee
NXP Employee

Hi Rineet

SD card which is working with the EVK board has ddr settings for EVK board,

which may not work on custom board. Uboot for custom board should be rebuilt

with new ddr calibration settings found from ddr test, put them in uboot/../mx6ul_14x14_evk/imximage.cfg

https://community.nxp.com/docs/DOC-105652 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

2,382 Views
rineet_kv
Contributor II

Hi Igor,

 we have rebuilt the UBOOT . It is working now. Thanks for your support

 Regards,

Rineet

0 Kudos
Reply