We are using IMX 6UL with boot device as SD card. Getting following error.
mmc_init: -110, time 1450
*** Warning - MMC init failed, using default environment
Same SD card is working with the EVK board. I have pasted the logs below.
U-Boot 2017.03-nxp/imx_v2017.03_4.9.11_1.0.0_ga+ga2fea67 (Aug 24 2018 - 12:43:48 +0530)
CPU: Freescale i.MX6UL rev1.2 528 MHz (running at 396 MHz)
CPU: Commercial temperature grade (0C to 95C) at 39C
Reset cause: POR
Model: Freescale i.MX6 UltraLite 14x14 EVK Board
Board: MX6UL 14x14 EVK
DRAM: 512 MiB
MMC: FSL_SDHC: 0, FSL_SDHC: 1
mmc_init: -110, time 1450
*** Warning - MMC init failed, using default environment
Display: TFT43AB (480x272)
Video: 480x272x24
In: serial
Out: serial
Err: serial
mmc_init: -110, time 1450
Net: No ethernet found.
Normal Boot
Hit any key to stop autoboot: 0
mmc_init: -110, time 1450
mmc_init: -110, time 1450
MMC: no card present
mmc_init: -123, time 2
Booting from net ...
No ethernet found.
No ethernet found.
Bad Linux ARM zImage magic!