Issue bitbake gstreamer1.0-plugins-bad

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Issue bitbake gstreamer1.0-plugins-bad

2,695 Views
veeranjaneyulug
Contributor III

Hi every one.

I gave below bitbake command but error

User1@FSETBLR1LX045:/media/veera/fsl-community-bsp/build$ bitbake gstreamer1.0-plugins-bad

Parsing recipes: 100% |########################################################################################################| Time: 00:01:04

Parsing of 2028 .bb files complete (0 cached, 2028 parsed). 2523 targets, 118 skipped, 1 masked, 0 errors.

NOTE: Resolving any missing task queue dependencies

NOTE: multiple providers are available for jpeg (jpeg, libjpeg-turbo)

NOTE: consider defining a PREFERRED_PROVIDER entry to match jpeg

Build Configuration:

BB_VERSION        = "1.24.0"

BUILD_SYS         = "x86_64-linux"

NATIVELSBSTRING   = "Ubuntu-12.04"

TARGET_SYS        = "arm-poky-linux-gnueabi"

MACHINE           = "imx6qsabresd"

DISTRO            = "poky"

DISTRO_VERSION    = "1.7"

TUNE_FEATURES     = "arm armv7a vfp neon callconvention-hard cortexa9"

TARGET_FPU        = "vfp-neon"

meta             

meta-yocto        = "(nobranch):f20e4c0cf6ddb29a1aad6e7b095e1472e81d330c"

meta-oe          

meta-multimedia   = "(nobranch):7bbacd0023fa1111da94ba0b2aafd7d872301ffe"

meta-fsl-arm      = "(nobranch):b74e5e690d8d4e149ea9de3f0fcca37bad93935f"

meta-fsl-arm-extra = "(nobranch):b32528c10caac5e85f2b5efe0e5b95322dd68ace"

meta-fsl-demos    = "(nobranch):48cb0bcdd226d2e7eee1fdc222713e1dff93342c"

meta-fsl-arm     

meta-fsl-demos    = "(nobranch):9a2973abf0d1de9742561c3af57de7b8cba7063a"

meta-browser      = "(nobranch):63963cc56c8d0291779693e62b66cb16e5c86883"

meta-gnome       

meta-networking  

meta-python      

meta-ruby        

meta-filesystems  = "(nobranch):7bbacd0023fa1111da94ba0b2aafd7d872301ffe"

meta-qt5          = "(nobranch):41c5daa84af4466bfc9aa61f6f772c68470a628b"

meta-multimedia   = "(nobranch):7bbacd0023fa1111da94ba0b2aafd7d872301ffe"

meta-fsl-qt5     

meta-fsl-bluez    = "(nobranch):9a2973abf0d1de9742561c3af57de7b8cba7063a"

NOTE: Preparing runqueue

NOTE: Executing SetScene Tasks

NOTE: Executing RunQueue Tasks

ERROR: Command Error: exit status: 126  Output:

/media/veera/fsl-community-bsp/build/tmp/sysroots/x86_64-linux/usr/bin/quilt: line 153: /home/User1/bin/bash: cannot execute binary file

ERROR: Function failed: patch_do_patch

ERROR: Logfile of failure stored in: /media/veera/fsl-community-bsp/build/tmp/work/x86_64-linux/gnu-config-native/20120814-r0/temp/log.do_patch.4211

ERROR: Command Error: exit status: 126  Output:

/media/veera/fsl-community-bsp/build/tmp/sysroots/x86_64-linux/usr/bin/quilt: line 153: /home/User1/bin/bash: cannot execute binary file

ERROR: Command Error: exit status: 126  Output:

/media/veera/fsl-community-bsp/build/tmp/sysroots/x86_64-linux/usr/bin/quilt: line 153: /home/User1/bin/bash: cannot execute binary file

ERROR: Function failed: patch_do_patch

ERROR: Logfile of failure stored in: /media/veera/fsl-community-bsp/build/tmp/work/x86_64-linux/autoconf-native/2.69-r11/temp/log.do_patch.4213

ERROR: Command Error: exit status: 126  Output:

/media/veera/fsl-community-bsp/build/tmp/sysroots/x86_64-linux/usr/bin/quilt: line 153: /home/User1/bin/bash: cannot execute binary file

ERROR: Function failed: patch_do_patch

ERROR: Logfile of failure stored in: /media/veera/fsl-community-bsp/build/tmp/work/x86_64-linux/automake-native/1.14.1-r0/temp/log.do_patch.4214

ERROR: Function failed: patch_do_patch

ERROR: Logfile of failure stored in: /media/veera/fsl-community-bsp/build/tmp/work/x86_64-linux/m4-native/1.4.17-r0/temp/log.do_patch.4212

ERROR: Task 70 (virtual:native:/media/veera/fsl-community-bsp/sources/poky/meta/recipes-devtools/automake/automake_1.14.1.bb, do_patch) failed with exit code '1'

ERROR: Task 63 (virtual:native:/media/veera/fsl-community-bsp/sources/poky/meta/recipes-devtools/autoconf/autoconf_2.69.bb, do_patch) failed with exit code '1'

ERROR: Task 348 (/media/veera/fsl-community-bsp/sources/poky/meta/recipes-devtools/m4/m4-native_1.4.17.bb, do_patch) failed with exit code '1'

ERROR: Task 94 (virtual:native:/media/veera/fsl-community-bsp/sources/poky/meta/recipes-devtools/gnu-config/gnu-config_20120814.bb, do_patch) failed with exit code '1'

NOTE: Tasks Summary: Attempted 27 tasks of which 23 didn't need to be rerun and 4 failed.

Waiting for 0 running tasks to finish:

Summary: 4 tasks failed:

  virtual:native:/media/veera/fsl-community-bsp/sources/poky/meta/recipes-devtools/automake/automake_1.14.1.bb, do_patch

  virtual:native:/media/veera/fsl-community-bsp/sources/poky/meta/recipes-devtools/autoconf/autoconf_2.69.bb, do_patch

  /media/veera/fsl-community-bsp/sources/poky/meta/recipes-devtools/m4/m4-native_1.4.17.bb, do_patch

  virtual:native:/media/veera/fsl-community-bsp/sources/poky/meta/recipes-devtools/gnu-config/gnu-config_20120814.bb, do_patch

Summary: There were 8 ERROR messages shown, returning a non-zero exit code.

How to solve this issue.can any body give some idea .

0 Kudos
Reply
3 Replies

1,959 Views
alejandrolozan1
NXP Employee
NXP Employee

Hi,

Which BSP version are you using? can you try to bitbake cleanall to target and retry?

/Alejandro

0 Kudos
Reply

1,959 Views
veeranjaneyulug
Contributor III

3.14.28 yocto linux kernel version

0 Kudos
Reply

1,959 Views
alejandrolozan1
NXP Employee
NXP Employee

Thanks,

Did you try to clean the previous bitbake?

Best Regards,

Alejandro

0 Kudos
Reply