Issue about not being able to proceed using the UsersGuide UsersGuide通りに作業を進められない件について

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Issue about not being able to proceed using the UsersGuide UsersGuide通りに作業を進められない件について

ソリューションへジャンプ
2,394件の閲覧回数
kokubu_hisatsug
Contributor I

Currently I am working on a project using the UsersGuide

(i.MX_Linux_User's_Guide.pdf ( Rev. L4.9.88_2.0.0-ga, 05/2018 )),

but I cannot get it to work the way it is written in the UsersGuide.

Please teach me how to fix this issue.

-UsersGuide(i.MX_Linux_User's_Guide.pdf ( Rev. L4.9.88_2.0.0-ga, 05/2018 ))

に従い作業を行っておりますが、想定の動作とならない現象が出ております。

解決方法をご教授下さい。

◆Current Evaluation Board: -使用している評価ボード

MCIMX6Q-SDB

◆Related Documents: -関連資料

i.MX_Linux_User's_Guide.pdf ( Rev. L4.9.88_2.0.0-ga, 05/2018 ))

◆Area of the issue in the document: -想定外結果となる箇所

Page 7, 「4.2.2 Using MfgTool」

◆Current state of the issue: -想定外の結果内容

After running the MfgTool2.exe

「No Device Connected」 is displayed.

 ※Attached image file: MfgTool2.png

 ※ Wanted Result: 「Done」

-MfgTool2.exeを実行後

「No Device Connected」と表示される

 ※参考添付資料名:MfgTool2.png

 ※期待値:Done

◆Additional Documents: -補足資料

 「iMX6_接続後.png」 →  This is an image of the Evaluation Board in the PC Device Manager.

 -「iMX6_接続後.png」 → PC上で認識されている評価ボードの状態

以上、何卒、宜しくお願い致します。

ラベル(1)
1 解決策
2,152件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi

reason for "No Device Connected" error may be computer

usb connection. Please try on other computer (preferably without usb 3.0 port),

try using external usb hub. May be useful to look at MFG Tool presentation on:

https://community.nxp.com/docs/DOC-328258 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

2 返答(返信)
2,153件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi

reason for "No Device Connected" error may be computer

usb connection. Please try on other computer (preferably without usb 3.0 port),

try using external usb hub. May be useful to look at MFG Tool presentation on:

https://community.nxp.com/docs/DOC-328258 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

2,152件の閲覧回数
kokubu_hisatsug
Contributor I

Thank you.

I changed PC(windows7-32bit USB2.0) and successful.



0 件の賞賛
返信