Issue about i.MX6DL Power Up

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Issue about i.MX6DL Power Up

1,273件の閲覧回数
tony_l_cai
Contributor III

Hi all,

     Our customized board cannot power up when press the ONOFF(button) for long time(time >6s).

why??  Could you give me some reasons? Is it a bug for this SoC?

3Q!

ラベル(3)
0 件の賞賛
返信
1 返信

1,197件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi tony

from sect.10.5 ONOFF (Button) IMX6DQRM :

When the chip main power supply is Off, a button press greater in duration than 750

ms asserts an output signal to request power from a power IC to power up the SoC..

Button presses greater than 5 seconds, when the SoC is powered, results in a direct

hardware power down request

It is recommended to check PMIC_ON_REQ signal

and that permanent SNVS voltage is provided to i.MX6.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信