Issue about GPIO on imx280

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Issue about GPIO on imx280

1,128 Views
tony_l_cai
Contributor III

Hi, all

     Do we have the  imx280 bsp porting user guide?

     could we have the tool like iomux.exe on imx280?

Labels (2)
0 Kudos
Reply
1 Reply

954 Views
igorpadykov
NXP Employee
NXP Employee

Hi tony

there is no iomux tool for i.MX28, one can use

Table 8-2. Pin Definitions MCIMX28RM

also it may be useful for development to look at

Application note sharing: Issues often met in i.MX28 application

Regarding porting guide, this depends on kernel version and may be used one

Linux 2.6.35 for i.MX53, MX53UG

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply