Issue about DDR options in Aid

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Issue about DDR options in Aid

1,499 Views
tony_l_cai
Contributor III

Hi,all

     Lot of the terminology I cannot seperate.Please help me.Following is :

     1. how to judge the number of the DRAM in ddr?

     2. in Aid, we can find the keyword "per CS", how to understand the CS? whether it means the DDR signal CS? And per DDR signal CS bit can contain 2 chip select. So in aid, whether per CS means the number of DDR signal CS bit or the number of the chips?

     3. how to understand the die? because in aid we can find the keyword "per die","single die", and how to know the number of the die in ddr?

     4. the relations or the differentials among the number of DRAM, Die, CS?

     and I'm so confused about these terminology when I fill the DDR aid.xls.

     help me,3q~ 

Labels (6)
0 Kudos
Reply
1 Reply

1,395 Views
igorpadykov
NXP Employee
NXP Employee

Hi tony

I would suggest to look at presentation describing this terminology

AMF-SDS-T0170  DRAM Controller Optimization for i.MX Application Processors

Freescale Technical Sessions Library|Freescale

one can ask help of local FAE for problems with access

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply