Issue About Power Manager on MX6DL

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Issue About Power Manager on MX6DL

1,152 Views
tony_l_cai
Contributor III

Hi,all

     I find a strange problem that when our board entered into sleep,from the log ,we found that once the board "sabresd_suspend_enter" then "sabresd_suspend_exit",why? log is following:

[  131.386809] ----suspend_enter----

[  131.387652] ---------max_timeout:0-----------

[  131.387658] power_suspend_late return 0

[  131.387668] PM: late suspend of devices complete after 0.847 msecs

[  131.387675] Disabling non-boot CPUs ...

[  131.388498] CPU1: shutdown

[  131.389154] ----syscore_suspend----

[  131.389292] -----sabresd_suspend_enter--------

[  131.389589] -----sabresd_suspend_exit--------

[  131.389833] Enabling non-boot CPUs ...

[  131.410766] CPU1: Booted secondary processor

[  131.410782] Calibrating delay loop (skipped) already calibrated this CPU

[  131.411156] i.MXC CPU frequency driver

[  131.411203] CPU1 is up

[  131.411800] PM: early resume of devices complete after 0.586 msecs

And this log has entered into suspend. You can see maybe it has exit suspend ? why?

Thanks~

Labels (3)
0 Kudos
Reply
1 Reply

1,067 Views
igorpadykov
NXP Employee
NXP Employee

Hi tony

processor will exit from low power mode if there is

enabled interrupt from some peripheral.

You can try to find it probably disabling some of them.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply