Issue About GPIO On MX6DL

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Issue About GPIO On MX6DL

1,309 Views
tony_l_cai
Contributor III

Hi,all

     Now,we find the gpio has some additional functions in kernel 3.10.35,as the following screenshot

pastedImage_1.png

I know the open drain,but I dont kown whether the GPIO can support the operation on MX6DL. And maybe I dont know what is OPEN SOURCE. Either I dont know the whether this operation can be used on MX6DL?

Thank you ~

Labels (3)
0 Kudos
Reply
1 Reply

1,218 Views
igorpadykov
NXP Employee
NXP Employee

Hi tony

i.MX6DL supports open drain, as described in Chapter 37

1.jpg

open source is not supported. Description can be found on

Push–pull output - Wikipedia, the free encyclopedia

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply