Issue About CS0_END

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Issue About CS0_END

1,794件の閲覧回数
tony_l_cai
Contributor III

Hi all,

        I get lot of info regarding to DDR2 2-channel settings in CS0_END, but I need the DDR3 1-channel settings in CS0_END, So how to set on MX6DL?

         And on my board, DDR3 1GB, the scripts show CS0_END=0x27 but as following:

pastedImage_0.png

the CS0_END should be 0x1f, so could you help me?

          

ラベル(3)
0 件の賞賛
返信
3 返答(返信)

1,635件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

MMDCx_MDASP[CS0_END] should be set to DDR_CS_SIZE/32MB + 0x7 (DDR base

address begins at 0x10000000).

That is, for 1GB CS0_END = 0x27


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

1,634件の閲覧回数
tony_l_cai
Contributor III

Hi Yuri,

From your description and the above, the size=(0x27+1)*256Mb /8=1280MB, but My total density is 1024MB, If the CS0_END=0x1F,I can understand, and It also can correspond to the chart. Why to enlarge?

And from your opinion, the base addr=0x1000 0000, the offset=1280MB, So the end addr=0x1014 0000?

Because I need to test DDR in uboot by uboot cmd "mtest",the start addr and end addr should be provided. I need to calc it, But actually, the physical memory is not so large, how to understand?

Thank you~

0 件の賞賛
返信

1,635件の閲覧回数
Yuri
NXP Employee
NXP Employee

Start address = 0x1000_0000

End address = 0x5000_0000 - 1

Regards,

Yuri

0 件の賞賛
返信