Is there some simple examples for how to use i.MX6q SDMA?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Is there some simple examples for how to use i.MX6q SDMA?

2,427 Views
uolli
Contributor III

Hi All,

I am leaning how the SDMA working on iMX6q CPU, but there are only few audio codec and uart examples in driver. i am wondering is there some simple example to show how the i.MX6q SDMA working theory?

i found mxc_sdma_memcopy_test.c in the  imx-test-3.0.35-4.0.0.tar.gz, but it is not working, always shows kernel NULL pointer error just like following shows

-------------

Unable to handle kernel NULL pointer dereference at virtual address 00000010

pgd = b874c000

[00000010] *pgd=4919b831, *pte=00000000, *ppte=00000000

Internal error: Oops: 17 [#8] PREEMPT SMP

Modules linked in: mxsdma [last unloaded: mxsdma]

CPU: 0    Tainted: G      D W    (3.0.15-g108480f-dirty #16)

PC is at sdma_write+0x2c4/0x354 [mxsdma]

LR is at sdma_write+0x2c0/0x354 [mxsdma]

pc : [<7f0183a4>]    lr : [<7f0183a0>]    psr: 60000013

sp : b872bf10  ip : 00000001  fp : 00000001

r10: 8b9004e0  r9 : 00000200  r8 : 00000000

r7 : 7f018c28  r6 : 7f018bf8  r5 : 7f018bdc  r4 : 00000400

r3 : 00000000  r2 : b8c6c000  r1 : 7f018434  r0 : 00000000

Flags: nZCv  IRQs on  FIQs on  Mode SVC_32  ISA ARM  Segment user

Control: 10c53c7d  Table: 4874c04a  DAC: 00000015

SP: 0xb872be90:

be90  00000000 80048aa0 00100100 00200200 b8c6c030 00000000 8b9004e0 18027000

beb0  18027400 0000040f 00000007 7f018bf8 7f018c28 8003fa10 00000000 7f018434

bed0  b8c6c000 00000000 00000400 7f018bdc 7f018bf8 7f018c28 00000000 00000200

bef0  8b9004e0 00000001 00000001 b872bf10 7f0183a0 7f0183a4 60000013 ffffffff

bf10  00000001 b90a9150 00000101 00000000 00000000 00000000 00000020 00000002

bf30  80a47d10 000083e0 b802da80 b8f1e000 00000000 7ea786fc b872bf80 00000000

bf50  b872a000 00000000 7ea78734 800e69c8 b872a000 b90a9150 b8f1e000 7ea786fc

bf70  00000000 00000000 00000000 800e6c38 00000000 00000000 2aae5568 00000000

R2: 0xb8c6bf80:

bf80  00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000

bfa0  00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000

bfc0  00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000

bfe0  00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000

c000  b81cee08 0000ffff 00000000 b8c6c000 00000000 00000000 00000000 00000000

c020  00000000 00000000 00000000 00000000 00000000 00000000 b8c6c038 b8c6c038

c040  00000000 ffdfe000 18001000 00000000 00000000 00000000 00000000 00000000

c060  00000000 00000000 00000000 00000000 00000000 00000000 b8c6d924 00000000

R10: 0x8b900460:

0460  00008000 00000000 ffffffff 8b900400 00000000 00000000 8b900478 8b900478

0480  000040c0 00000001 00100004 b8002a00 00000000 88026000 00100100 00200200

04a0  00008000 00000000 ffffffff 8b900480 00000000 00000000 800b7a14 00000002

04c0  00008000 00000000 ffffffff 8b900480 00000000 00000000 8b9004d8 8b9004d8

04e0  00008000 00000000 ffffffff 8b900480 00000000 00000000 8b9004f8 8b9004f8

0500  000040c0 00000001 0010000a b8002980 00000000 88028800 00100100 00200200

0520  00008000 00000000 ffffffff 8b900500 00000000 00000000 800b7a14 00000001

0540  00000000 00000000 ffffff80 00000001 00000000 00000000 80a8817c 80a8817c

Process sdma_test (pid: 5993, stack limit = 0xb872a2f0)

Stack: (0xb872bf10 to 0xb872c000)

bf00:                                     00000001 b90a9150 00000101 00000000

bf20: 00000000 00000000 00000020 00000002 80a47d10 000083e0 b802da80 b8f1e000

bf40: 00000000 7ea786fc b872bf80 00000000 b872a000 00000000 7ea78734 800e69c8

bf60: b872a000 b90a9150 b8f1e000 7ea786fc 00000000 00000000 00000000 800e6c38

bf80: 00000000 00000000 2aae5568 00000000 00000000 7ea78758 000083e0 00000004

bfa0: 800401c4 80040040 00000000 7ea78758 00000003 7ea786fc 00000000 7ea786fc

bfc0: 00000000 7ea78758 000083e0 00000004 00000000 00000000 2aae5000 7ea78734

bfe0: 00000000 7ea786f4 000084d8 2acebbac 40000010 00000003 00000000 00000000

[<7f0183a4>] (sdma_write+0x2c4/0x354 [mxsdma]) from [<800e69c8>] (vfs_write+0xa8/0x138)

[<800e69c8>] (vfs_write+0xa8/0x138) from [<800e6c38>] (sys_write+0x40/0x6c)

[<800e6c38>] (sys_write+0x40/0x6c) from [<80040040>] (ret_fast_syscall+0x0/0x30)

Code: e58db000 e59cc054 e12fff3c e59f107c (e5903010)

imx-ipuv3 imx-ipuv3.1: ext di clk already in use, go back to internal clk

BUG: scheduling while atomic: sdma_test/5993/0x00000002

Modules linked in: mxsdma [last unloaded: mxsdma]

[<80045d7c>] (unwind_backtrace+0x0/0xf8) from [<804c56b4>] (__schedule+0x4c0/0x6c0)

[<804c56b4>] (__schedule+0x4c0/0x6c0) from [<804c5e94>] (schedule_timeout+0x14c/0x1e8)

[<804c5e94>] (schedule_timeout+0x14c/0x1e8) from [<80076cb0>] (msleep+0x14/0x20)

[<80076cb0>] (msleep+0x14/0x20) from [<80373f38>] (ipu_init_sync_panel+0x134/0x12c8)

[<80373f38>] (ipu_init_sync_panel+0x134/0x12c8) from [<802468f8>] (mxcfb_set_par+0x384/0x4f0)

[<802468f8>] (mxcfb_set_par+0x384/0x4f0) from [<80246af8>] (mxcfb_blank+0x94/0xa8)

[<80246af8>] (mxcfb_blank+0x94/0xa8) from [<8022f308>] (fb_blank+0x3c/0x68)

[<8022f308>] (fb_blank+0x3c/0x68) from [<802390a8>] (fbcon_blank+0x1c4/0x258)

[<802390a8>] (fbcon_blank+0x1c4/0x258) from [<8026a090>] (do_unblank_screen+0x94/0x194)

[<8026a090>] (do_unblank_screen+0x94/0x194) from [<80220bc4>] (bust_spinlocks+0x24/0x4c)

[<80220bc4>] (bust_spinlocks+0x24/0x4c) from [<800439b0>] (die+0xa8/0x284)

[<800439b0>] (die+0xa8/0x284) from [<804c14c8>] (__do_kernel_fault.part.4+0x54/0x74)

[<804c14c8>] (__do_kernel_fault.part.4+0x54/0x74) from [<80049970>] (do_page_fault+0x2a4/0x30c)

[<80049970>] (do_page_fault+0x2a4/0x30c) from [<8003a408>] (do_DataAbort+0x34/0x9c)

[<8003a408>] (do_DataAbort+0x34/0x9c) from [<8003fa10>] (__dabt_svc+0x70/0xa0)

Exception stack(0xb872bec8 to 0xb872bf10)

bec0:                   00000000 7f018434 b8c6c000 00000000 00000400 7f018bdc

bee0: 7f018bf8 7f018c28 00000000 00000200 8b9004e0 00000001 00000001 b872bf10

bf00: 7f0183a0 7f0183a4 60000013 ffffffff

[<8003fa10>] (__dabt_svc+0x70/0xa0) from [<7f0183a4>] (sdma_write+0x2c4/0x354 [mxsdma])

[<7f0183a4>] (sdma_write+0x2c4/0x354 [mxsdma]) from [<800e69c8>] (vfs_write+0xa8/0x138)

[<800e69c8>] (vfs_write+0xa8/0x138) from [<800e6c38>] (sys_write+0x40/0x6c)

[<800e6c38>] (sys_write+0x40/0x6c) from [<80040040>] (ret_fast_syscall+0x0/0x30)

---[ end trace a0592d8c63058810 ]---

Segmentation fault

------------

for the details, check it out in this post https://community.freescale.com/message/337658#337658

thank you

Labels (6)
0 Kudos
Reply
3 Replies

1,796 Views
jamesbone
NXP TechSupport
NXP TechSupport

The examples and information that you found in the community link are the only available at the moment but I can recommend if you have an NDA within FSL please contact us, using the Service Request so we can provide more specific details of the SDMA

1,796 Views
uolli
Contributor III

thank you, Jamesbone

0 Kudos
Reply

1,796 Views
varsmolta
Contributor V

this blog here has good detail about imx sdma (imx5 and imx6 use same sdma peripheral) : Freescale i.MX51 SDMA tutorial (part I)