Is there any documentation available for USB over-current detection in i.MX6ul?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Is there any documentation available for USB over-current detection in i.MX6ul?

936件の閲覧回数
hardikbehere
Contributor I

Hi,

In our application, we are using over-current detection to control Vbus supply using Vbus enable pin.

But after detection of  USB over-current signal, processer assert a low signal to Vbus enable pin and remains low though USB device is removed from the device, we require to reboot the device to work USB again.

Regards,

Hardik Behere

ラベル(1)
0 件の賞賛
返信
1 返信

852件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Hardik

over-current one can check PP bit USB_nPORTSC1 description

in sect.54.6.31 Port Status & Control (USB_nPORTSC1) i.MX6UL Reference Manual

http://www.nxp.com/docs/en/reference-manual/IMX6ULRM.pdf

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信