Is there a bsp porting guide for the new yocto based dora bsp?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Is there a bsp porting guide for the new yocto based dora bsp?

1,389件の閲覧回数
scottwarner
Contributor III

Just curious if there was an updated bsp porting guide for dora release?  I can only find the older guide for the 3.0.35.x based releases.

Thanks

0 件の賞賛
返信
3 返答(返信)

1,121件の閲覧回数
LeonardoSandova
Specialist I

Hi Scott,

which guide are you referring to?

0 件の賞賛
返信

1,121件の閲覧回数
scottwarner
Contributor III

Sorry I should have mentioned that in the first post, it's the i.MX 6Dual/6Quad BSP Porting Guide.  We have a custom board that uses the sabresd board as a reference design.

Thanks

0 件の賞賛
返信

1,121件の閲覧回数
LeonardoSandova
Specialist I

Oh I see. I do not think there is  a guide :smileysad:

In the other hand, Yocto treats u-boot and kernel the same as any other recipes in the system. Do the corresponding patches on your u-boot and kernel repos; once you have this working, you need to create a layer and inside the corresponding recipes. As references, use the recipes for other upstream boards, take a look at

Freescale/meta-fsl-arm-extra · GitHub

0 件の賞賛
返信