Is there a Windows version of the HAB Code Signing Tool?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Is there a Windows version of the HAB Code Signing Tool?

1,212 Views
hughboddington
Contributor I

We're using the Secure Boot mode of the imx.6 but our toolchain is largely running under Windows.  Is there a Windows version of the Code Signing Tool, or even source that we could recompile?  We would be happy to spend money / sign an NDA / provide first-born child.

Labels (2)
0 Kudos
Reply
1 Reply

1,027 Views
igorpadykov
NXP Employee
NXP Employee

Hi Hugh

please refer to

Porting HAB cst tool to non-Linux platforms? 

in general for porting help one can try to apply to  NXP Professional Services:

http://www.nxp.com/support/nxp-professional-services:PROFESSIONAL-SERVICE
Pro-Support contact www.nxp.com/prosupport

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply