Is there a Linux driver for the Techpoint TP2855 video input chip available for iMX8MP Yocto

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Is there a Linux driver for the Techpoint TP2855 video input chip available for iMX8MP Yocto

4,588件の閲覧回数
TerryBarnaby1
Contributor V

We are producing a board using an IMX8MP which uses the Techpoint TP2855 video input chip. It appears the NXP Yocto kernel does not have a driver (I2C) for this chip.

Does anyone know if one is available somewhere ?

1 返信

4,584件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello TerryBarnaby1,

 

The NXP BSP does not include the TP2855, because it does not support in any of our EVK, but you can check with the community it is have:

http://freescale.github.io/

 

Regards

0 件の賞賛
返信