Is the ipu-lib able to work on iMX6Q?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Is the ipu-lib able to work on iMX6Q?

2,592 次查看
SamTan
Contributor I

I'm using the iMX6Q now. I want to add 3 screen layer in one display. I think the iMX6Q default code implement 2 screen layer fb0,fb1(overlay) in one display. How can I add the third screen layer?

I found iMX53 has ipu-lib and screenlayer library to meet this requirement. But in iMX6Q default code, the ipu-lib is useless.

标签 (1)
0 项奖励
回复
2 回复数

1,472 次查看
wayne1z
Contributor II

Ipu-lib is not used on i.mx6. Using GPU to do the third screen layer combination is better than IPU. The above mentioned ioctls are defined in include/linux/ipu.h. The unit test name is mxc_ipudev_test.out and also has a script named autorun-ipu.sh under the target rootfs.

0 项奖励
回复

1,472 次查看
fengwei
NXP Employee
NXP Employee

ipu-lib is not runnable on imx6, but you can directly use ioctl to get similar functions.

0 项奖励
回复