Is that okay to make ground unrouted polygon area of internal layer of PCB ?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Is that okay to make ground unrouted polygon area of internal layer of PCB ?

1,606 次查看
peteramond
Contributor V

Dear All,

I need some designing help regarding internal layer of PCB. Is that okay to make ground the unrouted polygon area of a PCB like follow ? I need to do this to make correct impedance of another layer routing traces.


Untitled.jpg
Are there any impact to this layer traces if I ground polygon area ?eter

Regards,
Peter.

标签 (4)
3 回复数

1,371 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Peter

yes it is okay to make ground, in general ground recommendations are described in

i.MX6 System Development User’s Guide sect.3.6.9 Ground plane recommendations

and Figure 3-27. Good layout GND plane detail

https://www.nxp.com/docs/en/user-guide/IMX6DQ6SDLHDG.pdf 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

1,371 次查看
peteramond
Contributor V

Hi igorpadykov

Many thanks for your reply.

But that section (3.6.9) is talking about different ground plane. Am I correct ?

But here I meant un routed area (Polygon area in ddr memory layout) Is that okay to make those polygon area to ground ?

hhh.jpg

Regards,

Peter.

0 项奖励
回复

1,371 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Peter

grounding unrouted area in the same layer also recommended,

it improves ESD and radiated emissions.

Best regards
igor

0 项奖励
回复