Is it possible to use a single 4.3 build to support Atheros and Intel Wifi PCI-e cards

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Is it possible to use a single 4.3 build to support Atheros and Intel Wifi PCI-e cards

837 次查看
michaelrobbelot
Contributor IV

All,

I was wondering if it was possible, despite the differences in drivers and wpa supplicants, to support both Atheros and Intel based Wifi PCI-e cards with a single 4.3 based build. In some cases, the cards also have Bluetooth support. Thanks.

Michael Robbeloth

标签 (2)
0 项奖励
回复
1 回复

731 次查看
jamesbone
NXP TechSupport
NXP TechSupport

I do not find any problems to have an Android Image with both drivers install to support both Wifi PCIe cards since only one of the cards it is going to be functional at time.   It is just like having a PC with both drivers and changing from one Wifi card to another.