Is it possible to configure iMX6 PCIE CX_ATU_MIN_REGION_SIZE?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Is it possible to configure iMX6 PCIE CX_ATU_MIN_REGION_SIZE?

跳至解决方案
1,518 次查看
andreaskarlsson
Contributor III

Hi,

Is it possible to configure iMX6 PCIE CX_ATU_MIN_REGION_SIZE? The RM is vague if it is or not. At one point in mention values between 4kB->64kB but not howto configure it.

49.10.45 iATU Region Lower Base Address Register(PCIE_PL_iATURLBA)

The CX_ATU_MIN_REGION_SIZE configuration parameter (Value Range: 4 kB, 8 kB,16 kB, 32 kB, 64 kB defaults to 64 kB)

Regards

Andreas

标签 (1)
标记 (2)
0 项奖励
回复
1 解答
1,351 次查看
igorpadykov
NXP Employee
NXP Employee

Hi andreas

not, this is fixed in hardware to 64 kB.

Best regards

igor

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,352 次查看
igorpadykov
NXP Employee
NXP Employee

Hi andreas

not, this is fixed in hardware to 64 kB.

Best regards

igor

0 项奖励
回复
1,351 次查看
andreaskarlsson
Contributor III

Ok, thanks

0 项奖励
回复