Is it possible to configure iMX6 PCIE CX_ATU_MIN_REGION_SIZE?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Is it possible to configure iMX6 PCIE CX_ATU_MIN_REGION_SIZE?

ソリューションへジャンプ
1,621件の閲覧回数
andreaskarlsson
Contributor III

Hi,

Is it possible to configure iMX6 PCIE CX_ATU_MIN_REGION_SIZE? The RM is vague if it is or not. At one point in mention values between 4kB->64kB but not howto configure it.

49.10.45 iATU Region Lower Base Address Register(PCIE_PL_iATURLBA)

The CX_ATU_MIN_REGION_SIZE configuration parameter (Value Range: 4 kB, 8 kB,16 kB, 32 kB, 64 kB defaults to 64 kB)

Regards

Andreas

ラベル(1)
タグ(2)
0 件の賞賛
返信
1 解決策
1,454件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi andreas

not, this is fixed in hardware to 64 kB.

Best regards

igor

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,455件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi andreas

not, this is fixed in hardware to 64 kB.

Best regards

igor

0 件の賞賛
返信
1,454件の閲覧回数
andreaskarlsson
Contributor III

Ok, thanks

0 件の賞賛
返信