Is it possible to change word size of EIM interface on runtime?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Is it possible to change word size of EIM interface on runtime?

Jump to solution
1,005 Views
JHY
Contributor IV

EIM interface can 8 or 16 bit word size.

Is it changable when running in linux?

Please tell me reference of adjusting word size in linux.

Thank you.

Labels (1)
Tags (1)
1 Solution
909 Views
Yuri
NXP Employee
NXP Employee

Hello,

  basically it is possible to reconfigure the EIM on-the-fly, but EIM

driver in NXP Linux is application dependent and should be implemented

by customers themselves. You may use EIM NOR Driver, described in
"i.MX_Linux_Reference_Manual.pdf" as an example. Linux IOCTL may be

used to reconfigure EIM options.    

Have a great day,

Yuri

------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct

Answer button. Thank you!

------------------------------------------------------------------------------

View solution in original post

1 Reply
910 Views
Yuri
NXP Employee
NXP Employee

Hello,

  basically it is possible to reconfigure the EIM on-the-fly, but EIM

driver in NXP Linux is application dependent and should be implemented

by customers themselves. You may use EIM NOR Driver, described in
"i.MX_Linux_Reference_Manual.pdf" as an example. Linux IOCTL may be

used to reconfigure EIM options.    

Have a great day,

Yuri

------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct

Answer button. Thank you!

------------------------------------------------------------------------------