Is it possible to bind Linux thread on each A53 of IMX8-MINI

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Is it possible to bind Linux thread on each A53 of IMX8-MINI

935 次查看
1561917549
Contributor I

大家好:

我们现在准备使用IMX8-MINI作为项目的处理器,请问该处理器是否支持在linux下把线程绑定到特定的A53核上使得该A53核只执行这一个线程?

举例:

A53-CPU0: Linux 线程1

A53-CPU1: Linux 线程2

Cortex-M4:保留

Hello ALL:

We have just started working on IMX8-MINI, will it be possible to  bind Linux thread on each A53 core of say quad-A53 scenario (not using M4 core for now).

For example:

A53-CPU0: Linux thread1

A53-CPU1: Linux thread2

Cortex-M4: Reserved

标签 (1)
0 项奖励
回复
1 回复

891 次查看
igorpadykov
NXP Employee
NXP Employee

Hi guoxian

one can try suggestions given on

How to run a program with only one CPU core? - Ask Ubuntu 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复