Is i.MX8M Mini Support ATF?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Is i.MX8M Mini Support ATF?

跳至解决方案
1,436 次查看
Hariharan1
Contributor III

Is that possible to flash Arm Trusted Firmware(ATF) without uboot?

If it is possible, what are the steps i have to follow?

 

Thanks,

0 项奖励
回复
1 解答
1,414 次查看
brian14
NXP TechSupport
NXP TechSupport

Hi @Hariharan1, 

Thank you for contacting NXP Support.

Based on the following official documentation from Trusted Firmware, the TF-A binary is combined with U-Boot. Therefore, using the NXP Tools to build the firmware you can't flash only this one.

7.21. NXP i.MX 8M Series — Trusted Firmware-A 2.10.0 documentation

I hope this information will be helpful.

Have a great day!

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,415 次查看
brian14
NXP TechSupport
NXP TechSupport

Hi @Hariharan1, 

Thank you for contacting NXP Support.

Based on the following official documentation from Trusted Firmware, the TF-A binary is combined with U-Boot. Therefore, using the NXP Tools to build the firmware you can't flash only this one.

7.21. NXP i.MX 8M Series — Trusted Firmware-A 2.10.0 documentation

I hope this information will be helpful.

Have a great day!

0 项奖励
回复