Hi community,
Our customer have a question about i.MX6SDL EIM.
They consider using EIM continuous BCLK, but didn't understand whether address is incremented when using continuous BCLK.
Would you let me know it?
Best Regards,
Satoshi Shimoda
Solved! Go to Solution.
 
					
				
		
 Yuri
		
			Yuri
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		Hello,
In synchronous mode, after address assertion, a burst of sequential
data can be accessed, assuming address incrementing is provided
by an external device (internally). Start address of the burst is provided 
by i.MX6 master. Burst length is configured in EIM. From section 22.5.4 
(Burst Mode (Synchronous) Memory Operation) of the i.MX6 S/DL RM :
 “When this mode is set, the controller attempts to translate the Master burst 
accesses to memory burst accesses, being limited by the memory burst length, 
predefined by BL value, or memory and Master WRAP/INCR boundary crossing 
non-matching. Only the first address accessed is put by the controller on the external 
address bus in a memory burst sequence.” 
The continuous mode is differ from single burst in such manner that
the clock is not stopped right after burst finish.
Have a great day,
Yuri
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
 
					
				
		
 Yuri
		
			Yuri
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		Hello,
In synchronous mode, after address assertion, a burst of sequential
data can be accessed, assuming address incrementing is provided
by an external device (internally). Start address of the burst is provided 
by i.MX6 master. Burst length is configured in EIM. From section 22.5.4 
(Burst Mode (Synchronous) Memory Operation) of the i.MX6 S/DL RM :
 “When this mode is set, the controller attempts to translate the Master burst 
accesses to memory burst accesses, being limited by the memory burst length, 
predefined by BL value, or memory and Master WRAP/INCR boundary crossing 
non-matching. Only the first address accessed is put by the controller on the external 
address bus in a memory burst sequence.” 
The continuous mode is differ from single burst in such manner that
the clock is not stopped right after burst finish.
Have a great day,
Yuri
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
 
					
				
		
Dear Yuri,
Thank you for your reply.
According to your reply, the address signal from i.MX6 is not incremented, so external device have to increment internally by its own, right?
Best Regards,
Satoshi Shimoda
 
					
				
		
 Yuri
		
			Yuri
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		Hello,
>  the address signal from i.MX6 is not incremented, so external device 
> have to increment internally by its own, right? 
Correct.
Regards,
Yuri.