Is Write Leveling required for all DDR3?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Is Write Leveling required for all DDR3?

1,825件の閲覧回数
victorsv1978
Contributor I

So we have a development project that used iMX6 and 4 modules of DDR3. There is a note on the schematic about bit swapping  on low order bit of each byte must reside at bit 0 of the byte. Somehow, this was not followed by our third party PCB layout designer and he designed it as below. The PCB is now manufactured and being assembled at our SMT line. With the bit swapping issue, obviously we can not do write calibration. 

My question is, does write calibration always required for DDR3? Can we still use the finished PCB to continue with our development?

pastedImage_1.png

ラベル(1)
タグ(1)
0 件の賞賛
返信
2 返答(返信)

1,685件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Vic

finding optimal timings with write calibration improves

system stability, in general one can use ddr settings for

nxp reference boards with similar configuration.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

1,685件の閲覧回数
victorsv1978
Contributor I

Hi Igor,

That you for your answer, that clarifies a lot. However, how can we use DDR settings from the reference boards and apply it to our design? Do you have any documentation how is it done?

Thanks,

Vic

0 件の賞賛
返信