Is Wi-Fi Direct[p2p] Support in Android 7 ?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Is Wi-Fi Direct[p2p] Support in Android 7 ?

6,094 次查看
ThanarajS
Contributor III

Hi All,

  We want to know the Wi-Fi Direct Support is there or not in Android 7 Released BSP version 7.1.1_1.0.0?

  Can we get Wi-Fi Direct Supported BSP Source?

   Interfaces:

      As per android, Wi-Fi Direct will support with Normal Wi-Fi Mode only.

      If we want to enable wifi direct, wifi should be enabled then only we can use wifi direct.

      So is there separate interface is created for Wi-Fi[wlan0] & Wi-Fi Direct[p2p0] or It will work with one interface[wlan0] ?

Thanks in Advance!!!!

Regrads,

Raj.

Regards,
Thanaraj Subramani
标签 (5)
0 项奖励
回复
4 回复数

5,421 次查看
aravinthkumarja
Senior Contributor II

Hi Raj,

Check Section 28 on the attached documet.

Regards,

Aravinth

0 项奖励
回复

5,421 次查看
ThanarajS
Contributor III

Hi Aravinth,

   I didn't get any attachment in previous mail. Could you please send once?

Regards,

Thanaraj.

Regards,
Thanaraj Subramani
0 项奖励
回复

5,421 次查看
joanxie
NXP TechSupport
NXP TechSupport

The WiFI Direct is enabled by default in n7.1.1 release for BCM4339 WiFi chip. You can find it in Settings->WiFi->More.

0 项奖励
回复

5,421 次查看
aravinthkumarja
Senior Contributor II

PFA.

0 项奖励
回复