Is USART supported on i.MX93?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Is USART supported on i.MX93?

Jump to solution
2,172 Views
Takashi_Kashiwagi
Senior Contributor I

Hi Community!

I have a question about the I/O installed in i.MX93.

Is USART(not UART) supported on i.MX93?(Something with serial clock input/output like the one installed in i.MXRT600)

 

I checked IMX93RM.pdf. Looking at "Figure 1.Simplified Block Diagram", it looks like a total of 8 UARTs/USARTs are installed. But "Chapter 62 Low Power Universal Asynchronous Receiver/Transmitter (LPUART)" does not seem to have any description of USART.
Or is it written in another chapter?

Similarly, IMX93CEC.pdf did not have USART listed.

Best Regards,

KASHIWAGI Takashi

0 Kudos
Reply
1 Solution
2,101 Views
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Hi @Takashi_Kashiwagi 

Does that mean that "Figure 1.Simplified Block Diagram" in IMX93RM.pdf and the block diagram in product page  are a typo? 

-->Yes,i think so as there is no such function description in RM.

Best Regards

Zhiming

View solution in original post

4 Replies
2,136 Views
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Hi @Takashi_Kashiwagi 

Please refer Chapter 62 Low Power Universal Asynchronous Receiver/Transmitter (LPUART), no USART support.

0 Kudos
Reply
2,130 Views
Takashi_Kashiwagi
Senior Contributor I

Hi @Zhiming_Liu - san

 

Thank you for reply.

 

Please refer Chapter 62 Low Power Universal Asynchronous Receiver/Transmitter (LPUART), no USART support.

I see. Does that mean that "Figure 1.Simplified Block Diagram" in IMX93RM.pdf and the block diagram in product page  are a typo? 

The block diagram is written as if the i.MX93 is equipped with a USART module.

 

Best Regards.

KASHIWAGI Takashi.

 

0 Kudos
Reply
2,102 Views
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Hi @Takashi_Kashiwagi 

Does that mean that "Figure 1.Simplified Block Diagram" in IMX93RM.pdf and the block diagram in product page  are a typo? 

-->Yes,i think so as there is no such function description in RM.

Best Regards

Zhiming

2,076 Views
Takashi_Kashiwagi
Senior Contributor I

Hi @Zhiming_Liu - san

 

Thank you for reply!

 

Yes,i think so as there is no such function description in RM.

I understand. 

 

Best Regards

KASHIWAGI Takashi

0 Kudos
Reply