Is CONFIG_IMX_HAB option in U-Boot unbootable from NAND without burning fuses in i.MX6?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Is CONFIG_IMX_HAB option in U-Boot unbootable from NAND without burning fuses in i.MX6?

ソリューションへジャンプ
4,816件の閲覧回数
JohnKlug
Senior Contributor I

We are trying to go as far as we can with HAB without burning fuses, as we have very few boards working so far in our project.

If I add CONFIG_IMX_HAB to U-Boot without blowing fuses, U-Boot boots from USB, but not from NAND flash (no console messages).  If I burn without CONFIG_IMX_HAB, with the same uuu.auto, everything works great.

Are there fuse requirements to boot CONFIG_IMX_HAB enabled U-Boot?

I am using identical uuu.auto files except for the U-Boot image in both the working and non-working cases.  Something must have been written to flash, because when I boot, the Freescale USB device does not show up on my PC.

I used the U-Boot menuconfig program to add HAB to U-Boot.  The following lines were added to U-Boot (not shown in context):

CONFIG_IMX_HAB=y
# CONFIG_FSL_MFGPROT is not set
CONFIG_SYS_FSL_HAS_SEC=y
CONFIG_SYS_FSL_SEC_COMPAT=4

 

0 件の賞賛
返信
1 解決策
4,727件の閲覧回数
JohnKlug
Senior Contributor I

Here is the solution to the problem I was having.  Word 0x24 of the U-Boot image gives the length of the U-Boot image after signing:

$ od -j 0x24 -N4 -An -X u-boot.imx
 000a4060
objcopy -I binary -O binary --pad-to 0xa4060 --gap-fill=0xff u-boot-nand-signed.imx  u-boot-nand-signed-pad.imx

Without the padding, the boot fails.

元の投稿で解決策を見る

7 返答(返信)
4,728件の閲覧回数
JohnKlug
Senior Contributor I

Here is the solution to the problem I was having.  Word 0x24 of the U-Boot image gives the length of the U-Boot image after signing:

$ od -j 0x24 -N4 -An -X u-boot.imx
 000a4060
objcopy -I binary -O binary --pad-to 0xa4060 --gap-fill=0xff u-boot-nand-signed.imx  u-boot-nand-signed-pad.imx

Without the padding, the boot fails.

4,609件の閲覧回数
BenSu
Contributor III

That's great, JohnKlug.

I pad the image and it boots up.

Why NXP does not list the option out?

Thanks

BR

Ben

0 件の賞賛
返信
4,811件の閲覧回数
JohnKlug
Senior Contributor I

Related to how to test things without burning fuses, I see the following in U-Boot help:

hab_failsafe- run BootROM failsafe routine

 

So is it possible to set the fuse shadow registers, execute the hab_failsafe command, and get a secure boot to be simulated without burning fuses?  Is this documented anywhere?

0 件の賞賛
返信
4,794件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

refer to the uboot source code, you can set sec_boot=y in the uboot via define the CONFIG_AHAB_BOOT to enable AHAB

#ifdef CONFIG_AHAB_BOOT

#define AHAB_ENV "sec_boot=yes\0"

#else

#define AHAB_ENV "sec_boot=no\0"

#endif

 

"https://source.codeaurora.org/external/imx/uboot-imx/tree/include/configs/imx8qxp_mek.h?h=imx_v2020...."

 

0 件の賞賛
返信
4,785件の閲覧回数
JohnKlug
Senior Contributor I

CONFIG_AHAB_BOOT is an i.MX8 AHAB feature according to U-Boot.  i.MX6 is not mentioned.

It would be nice if there was an up to date document on how to build U-Boot and sign it for the i.MX6ULL processor.

0 件の賞賛
返信
4,776件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

for imx6, one can use CONFIG_SECURE_BOOT in the board.h file to enable the security boot in uboot

0 件の賞賛
返信
4,608件の閲覧回数
BenSu
Contributor III

"Steps must be taken to remove support in customer application software if the end product is not using HAB API at all.
For instance, U-Boot users must ensure CONFIG_SECURE_BOOT is not being selected in their build environment."

That's in point 3 in section 5 Security considerations in AN12263.pdf.

Can we enable CONFIG_SECURE_BOOT?

BR

Ben

0 件の賞賛
返信