Ipu Initialization

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Ipu Initialization

1,349件の閲覧回数
muhammadasif
Contributor I

With i.mx6dl display (ipu and ldb) after initialization, there is nothing on screen until we set these two memory areas with these values:
*0x02760060=0x00008805;
*0x02780064=0x0380;
After writing these values display works properly. In processor reference manual of imx6dl, these memory areas come under the address space of ipu memory mapping which we can not access via ipu registers. Can anyone please describe how can we achieve such settings using ipu registers? we need to have these values for our display to work correctly.

Thank you very much in advance.

0 件の賞賛
返信
1 返信

1,238件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

please look at the following

https://community.nxp.com/message/581155 

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信