Iperf server crash on FEC

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Iperf server crash on FEC

1,713 Views
parth_shah
Contributor III

We have a custom Hardware where in i.MX6SoloX processor is being used. A microchip KSZ9477 ethernet switch IC is interfaced with processor using RGMII interface to FEC1 controller of i.MX6SoloX processor. The Linux kernel version 4.14.200 is being used. We have enabled CONFIG_1588_PTP.

The KSZ9477 ethernet switch driver is available at following location:

https://github.com/Microchip-Ethernet/EVB-KSZ9477/tree/master/KSZ/linux-drivers/ksz9897/linux-4.14/d...

We are connecting 2 such customer hardware and making them client and server. 

To check the network performance, we are using iperf3. But we see a crash on iperf3 server. Please find attached logs.

We suspect that this crash is because of PTP is enabled in both FEC controller and KSZ9477 Switch driver.

Any suggestion is highly appreciated.

Labels (1)
Tags (2)
0 Kudos
Reply
0 Replies