Interrupts in i.MX6UL

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Interrupts in i.MX6UL

991 次查看
surendrajadhav
Contributor IV

Hello,

Let me know which pins of the i.MX6UL processor I can use for interrupts. I saw in one EVK board where they are using SNVS_TAMPER pins for interrupt input from Ethernet.

As there are no dedicated pins being observed, let me know if I can use SNVS_TAMPER pins for interrupt.

Regards,

Surendra Jadhav

0 项奖励
回复
1 回复

822 次查看
Yuri
NXP Employee
NXP Employee

Hello,

 

The i.MX6UL tamper pins are configured for GPIO or tamper functionality

via fuses. Please look athttps://community.nxp.com/thread/382019 

 

 Note : If TAMPER_PIN_DISABLE[1:0] fuse is programmed to "11 - disabled
TAMPER0-9 used as GPIO", then the tamper pins are in gpio mode, you do not
need to configure iomux.

  When in GPIO mode, the tamper pins can operate as interrupts sources.

Please use the i.MX6 Reference Manual, Chapter 26 [General Purpose Input/Output
(GPIO) ].

Have a great day,

Yuri

 

------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct

Answer button. Thank you!

0 项奖励
回复