Internal watchdog question on i.MX6

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Internal watchdog question on i.MX6

1,439件の閲覧回数
charleshuang
Senior Contributor II

Hi Freescale,

Let GPIO_9 pin sets WDOG1_B. When internal watchdog on i.MX6 Dual-Core CPU is timeout, this pin will be action.

If some problems occur on CPU and internal watchdog is timeout, this pin will have action it?

Thank you.

Best Regards,

Alex

ラベル(3)
0 件の賞賛
返信
3 返答(返信)

1,141件の閲覧回数
Yuri
NXP Employee
NXP Employee

  Correct, GPIO_9 pin may be asserted, when the watchdog (WDOG1) event
takes place. It should be configured as WDOG1_B :

IOMUXC_SW_MUX_CTL_PAD_GPIO09[MUX] = 1


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

1,141件の閲覧回数
charleshuang
Senior Contributor II

Hi Yuri,

1. I read i.MX 6Dual/6Quad Applications Processor Reference Manual file. According to this document, if I want GPIO_9 pin to configured as WDOG1_B.

It is set as follows:

Pad Mux Register (IOMUXC_SW_MUX_CTL_PAD_GPIO09):

001 ALT1 — Select signal WDOG1_B. (IOMUXC_SW_MUX_CTL_PAD_GPIO09[MUX] = 1)

But I do not see the following message should be set:

IOMUXC_KEY_COL6_SELECT_INPUT[DAISY] = 0 (for mode ALT2)

Do I need to set the above message?

2. No matter what the circumstances, when the internal watchdog is timeout, this pin must be operating.

   Correct?

Thank you.

Best Regards,

Alex Cheng

0 件の賞賛
返信

1,141件の閲覧回数
Yuri
NXP Employee
NXP Employee

Correct, the daisy chain is not used for outputs.

Rrgards,

Yuri.

0 件の賞賛
返信