Internal pull-ups on i.MX6 Solo X processor.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Internal pull-ups on i.MX6 Solo X processor.

2,574件の閲覧回数
achyut_hegde
Contributor III

We are trying to find out the internal pull-up resistors on the IMX6 processor.

From the data sheet it is not clear whether there are any pull-ups present inside the processor on SDIO lines(0:6)

D0-D3 including the CMD and CLOCK lines.

We are designing a system with a peripheral which is running in high speed SDIO mode connected to imx6 processor which needs to take into account the voltage levels achieved on these lines.

ラベル(1)
0 件の賞賛
返信
1 返信

2,409件の閲覧回数
gusarambula
NXP TechSupport
NXP TechSupport

Hello Achyut Hegde,

You can find the pull resistor enablement and options on the pad configuration registers on the i.MX6SX Reference Manual (link below, you may need to login to download this document).

https://www.nxp.com/webapp/Download?colCode=IMX6SXRM

The properties would be PKE (Pull/Keep Enable Field), PUE (Pull/Keep Select Field) and PUS (Pull Up/Down Config. Field).

I hope this helps!
Regards,

0 件の賞賛
返信