Interfacing a parallel image sensor to i.mx 7ulp with FlexIO

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Interfacing a parallel image sensor to i.mx 7ulp with FlexIO

2,247 Views
kunf
Contributor II

Does any one have experience with Interfacing 8bit parallel Image sensor to i.mx 7ulp with FlexIO?

What is the maximum possible resolution with e.g. YUV422 or RGB888?

Thanks for your help

 

 

Labels (1)
0 Kudos
Reply
3 Replies

2,236 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello kunf,

 

The MX7ULP has MIPI for camera interface, if you want to interface flexio you have to develop the interface with gpio.

 

Regards

0 Kudos
Reply

2,227 Views
kunf
Contributor II

Thank you for your answer. according to the reference manual, the i.mx 7ulp (in contrast to the solo and dual variants) does not have a MIPI camera interface. The only camera interface available is the VIU, which has only very limited options for the maximum possible resolution. Therefore my question is whether a camera stream of higher quality can be achieved via the FlexIO module and GPIOs.

 

Regards

0 Kudos
Reply

2,221 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

The MX7ULP has MIPI DSI not for camera, for camera it has parallel IF/F. No you can not connect the camera with high resolution through FlexIO.

Regards

0 Kudos
Reply