Interfacing a parallel image sensor to i.mx 7ulp with FlexIO

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Interfacing a parallel image sensor to i.mx 7ulp with FlexIO

2,206件の閲覧回数
kunf
Contributor II

Does any one have experience with Interfacing 8bit parallel Image sensor to i.mx 7ulp with FlexIO?

What is the maximum possible resolution with e.g. YUV422 or RGB888?

Thanks for your help

 

 

ラベル(1)
0 件の賞賛
返信
3 返答(返信)

2,195件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello kunf,

 

The MX7ULP has MIPI for camera interface, if you want to interface flexio you have to develop the interface with gpio.

 

Regards

0 件の賞賛
返信

2,186件の閲覧回数
kunf
Contributor II

Thank you for your answer. according to the reference manual, the i.mx 7ulp (in contrast to the solo and dual variants) does not have a MIPI camera interface. The only camera interface available is the VIU, which has only very limited options for the maximum possible resolution. Therefore my question is whether a camera stream of higher quality can be achieved via the FlexIO module and GPIOs.

 

Regards

0 件の賞賛
返信

2,180件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

The MX7ULP has MIPI DSI not for camera, for camera it has parallel IF/F. No you can not connect the camera with high resolution through FlexIO.

Regards

0 件の賞賛
返信