Interfacing SRAM of FPGA using EIM Module.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Interfacing SRAM of FPGA using EIM Module.

2,367 Views
shammi112
Contributor I

Hello,

I am trying to interface SRAM on EIM interface of imx6. I am using linux 4.1. Does it require specific driver to handle the SRAM. Is there any reference dts file.

Regards,

SHAMMI

0 Kudos
Reply
1 Reply

2,128 Views
igorpadykov
NXP Employee
NXP Employee

Hi SHAMMI

one can refer to imx6qdl-sabreauto.dtsi "weim_nor" example

linux-imx.git - i.MX Linux Kernel 

and description in Chapter 41 EIM NOR Driver attached Linux Manual.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply