Interfacing SRAM of FPGA using EIM Module.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Interfacing SRAM of FPGA using EIM Module.

2,370件の閲覧回数
shammi112
Contributor I

Hello,

I am trying to interface SRAM on EIM interface of imx6. I am using linux 4.1. Does it require specific driver to handle the SRAM. Is there any reference dts file.

Regards,

SHAMMI

0 件の賞賛
返信
1 返信

2,131件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi SHAMMI

one can refer to imx6qdl-sabreauto.dtsi "weim_nor" example

linux-imx.git - i.MX Linux Kernel 

and description in Chapter 41 EIM NOR Driver attached Linux Manual.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信