Interfacing FPGA SDIO interface with imx6 SD3

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Interfacing FPGA SDIO interface with imx6 SD3

1,753 Views
shammi112
Contributor I

Hello,

We are  trying to interface FPGA using sdio interface on imx6 sd3 interface. But imx6 is not able to detect FPGA SLAVE device. we are getting the below errors.

43.136538] mmc1: queuing unknown CIS tuple 0x01 (0 bytes)
[ 56.955815] mmc1: error -22 whilst initialising SDIO card
[ 59.026637] mmc1: error -110 whilst initialising SDIO card
[ 61.096092] mmc1: error -110 whilst initialising SDIO card
[ 63.166095] mmc1: error -110 whilst initialising SDIO card

Regards,

SHAMMI

0 Kudos
Reply
1 Reply

1,528 Views
art
NXP Employee
NXP Employee

Most likely, it means that your FPGA is not configured properly to be recognized as an SDIO device. Please check your FPGA configuration first.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply