Interfacing Async NAND with iMX6Q

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Interfacing Async NAND with iMX6Q

ソリューションへジャンプ
2,290件の閲覧回数
atillametetured
Contributor V

Greetings,

We are prepearing a custom HW with an Async Single Die Nand Flash and eMMC. By looking at Sabre for Smart Devices schematics, it is easy to figure out the eMMC connection. We used the  same connections as Sabre did. However looking at Sabre AI board for NAND connections, I cant figure where W/R#, CLK/WE# and WP# pins of the NAND Flash should go. Are they meant for GPIO or do they have a designated connection point on imx?

Thanks in advance

Mete

ラベル(2)
0 件の賞賛
返信
1 解決策
2,168件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Atilla

these signals can be found in Table 29-1. GPMI External Signals

i.MX6DQ Reference Manual

http://cache.freescale.com/files/32bit/doc/ref_manual/IMX6DQRM.pdf

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

2 返答(返信)
2,169件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Atilla

these signals can be found in Table 29-1. GPMI External Signals

i.MX6DQ Reference Manual

http://cache.freescale.com/files/32bit/doc/ref_manual/IMX6DQRM.pdf

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

2,168件の閲覧回数
atillametetured
Contributor V

Hello Igor,

Thank you. I will consider the manual.

Regards,

Atilla

0 件の賞賛
返信