Integration Support for ov5645 camera over mipi-csi2 interface

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Integration Support for ov5645 camera over mipi-csi2 interface

3,810 Views
parveenkumaryad
Contributor III

Hi All,

We are trying to integrate ov5645 camera over MIPI-CSI2 interface on imx6q/d-sabre-SDP board. We are trying to stream video at 720p@30 fps, also capture still image through the camera.

Can anyone provide us the integration steps or guide for the camera registration and settings?

What configuration do we need to change for the camera integration in the kernel?

Can anyone provide the register configuration for 1280X720p resolution at 30fps?

0 Kudos
Reply
1 Reply

2,244 Views
Yuri
NXP Employee
NXP Employee

Please use the next :


“Some Experience When Enable MIPI Camera”

< https://community.freescale.com/thread/307065 >

< https://community.freescale.com/servlet/JiveServlet/download/328301-262515/Debug%20steps%20for%20cus... >
 

Also, please refer to Linux documentation, in particular :
Chapter 21 (MIPI CSI2 Driver)
and

Chapter 9 [Video for Linux Two (V4L2) Driver ]

of “i.MX_6_Linux_Reference_Manual.pdf”.


http://www.freescale.com/webapp/Download?colCode=L3.10.17_1.0.0_IMX6QDLS_BUNDLE&appType=license&loca...

Summary Page link :


http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=IMX6_SW


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply