Integrating GPU with X11 in imx6q

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Integrating GPU with X11 in imx6q

跳至解决方案
1,542 次查看
VAISAKH
Contributor II

Hello ,

What I have to do for integrating the GPU ( Opend EGLS) with x11.. ?

Please see my observations

I am using sabrelite board ( imx6q ) . In that GPU is tested and its working .

Also I did Xserver setup  (startx)

After that I compiled a EGL example from SimpleGL example - maemo.org wiki

root@freescale /$ export DISPLAY=0:0

root@freescale /$ ./EGLSample

Connected to X SERVER

X Error of failed request:  BadAtom (invalid Atom parameter)

Major opcode of failed request:  18 (X_ChangeProperty)

Atom id in failed request:  0x0

Serial number of failed request:  11

Current serial number in output stream:  12

--------------------------------------------------------------------

please help me

~Vaisakh N


标签 (2)
0 项奖励
回复
1 解答
1,012 次查看
andre_silva
NXP Employee
NXP Employee
0 项奖励
回复
2 回复数
1,012 次查看
YixingKong
Senior Contributor IV

Vaisakh, please click Correct Answer if Andre's answer is good one.

Thanks,

Yixing

0 项奖励
回复
1,013 次查看
andre_silva
NXP Employee
NXP Employee
0 项奖励
回复