Hi
I am using ubuntu 11.10 as host system and succesfully build a new images for ubuntu ( u-boot.bin, uImage, anf file system) for I.MX53 QSB, using the steps mentioned in CreateUbuntu1110ltib110901.docx, however i could not install git-core,and i could not find /etc/inetd.conf in my host system.
neither i could not start the board with these new images, nor anything is coming at minicom can any one tell me what could be the resaon for this.
However I just needed the new uImage so I used u-boot-mx53-loco.bin which is prebuilt image given by freescale, after this i could see booting happening but it fails to load file system, the log is like this
**********************************************************************************************************************************************
EXT3-fs: barriers not enabled
kjournald starting. Commit interval 5 seconds
EXT3-fs (mmcblk0p1): using internal journal
EXT3-fs (mmcblk0p1): recovery complete
EXT3-fs (mmcblk0p1): mounted filesystem with writeback data mode
VFS: Mounted root (ext3 filesystem) on device 179:1.
Freeing init memory: 172K
starting pid 1210, tty '': '/etc/rc.d/rcS'
Mounting /proc and /sys
Starting the hotplug events dispatcher udevd
Synthesizing initial hotplug events
Setting the hostname to freescale
Mounting filesystems
cp: write error: No space left on device
cp: write error: No space left on device
cp: write error: No space left on device
cp: write error: No space left on device
cp: write error: No space left on device
cp: write error: No space left on device
mount: mounting usbfs on /proc/bus/usb failed: No such file or directory
starting pid 2257, tty '': '/sbin/getty -L ttymxc0 115200 vt100
arm-none-linux-gnueabi-gcc (4.4.4_09.06.2010) 4.4.4
root filesystem built on Sat, 23 Mar 2013 18:32:24 +0530
Freescale Semiconductor, Inc.
freescale login:
**********************************************************************************************************************************************
Can any one tell me resons for these two problems
Solved! Go to Solution.
Please apply the BSP 11.09 patch.
You can download the BSP and patch from the i.MX53QSB web page:
http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=IMX53QSB&fpsp=1&tab=Design_Tools_Tab
BSP : L2.6.35_11_09_ER_SOURCE
Patch : IMX53_LINUX_1109_BSP_PATCH
Also, you can try the "MX53_QSB_UBUNTU_SD_DEMO_IMAGE". It contain the Ubuntu filesystem for i.MX53QSB.
I again tried to build images for IMX53 QSB with different kernel version 2.6.38 using LTIB, but with this, building failed
with this log
************************************************************************************************************************************************************
make[1]: *** [ScreenLayer.o] Error 1
make[1]: Leaving directory `/home/praveen/L2.6.35_11.09.01_ER_source_bundle/ltib/rpm/BUILD/imx-lib-11.09.01/screenlayer'
make: *** [screenlayer] Error 2
error: Bad exit status from /home/praveen/L2.6.35_11.09.01_ER_source_bundle/ltib/tmp/rpm-tmp.96851 (%build)
RPM build errors:
Bad exit status from /home/praveen/L2.6.35_11.09.01_ER_source_bundle/ltib/tmp/rpm-tmp.96851 (%build)
Build time for imx-lib: 6 seconds
Failed building imx-lib
f_buildrpms() returned an error, exiting
traceback:
main:560
Started: Mon Mar 25 15:49:58 2013
Ended: Mon Mar 25 16:13:00 2013
Elapsed: 1382 seconds
These packages failed to build:
imx-lib
Build Failed
Exiting on error or interrupt
************************************************************************************************************************************************************
I am attaching complete log
Please apply the BSP 11.09 patch.
You can download the BSP and patch from the i.MX53QSB web page:
http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=IMX53QSB&fpsp=1&tab=Design_Tools_Tab
BSP : L2.6.35_11_09_ER_SOURCE
Patch : IMX53_LINUX_1109_BSP_PATCH
Also, you can try the "MX53_QSB_UBUNTU_SD_DEMO_IMAGE". It contain the Ubuntu filesystem for i.MX53QSB.