Integrating GPU with X11 in imx6q

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Integrating GPU with X11 in imx6q

Jump to solution
1,298 Views
VAISAKH
Contributor II

Hello ,

What I have to do for integrating the GPU ( Opend EGLS) with x11.. ?

Please see my observations

I am using sabrelite board ( imx6q ) . In that GPU is tested and its working .

Also I did Xserver setup  (startx)

After that I compiled a EGL example from SimpleGL example - maemo.org wiki

root@freescale /$ export DISPLAY=0:0

root@freescale /$ ./EGLSample

Connected to X SERVER

X Error of failed request:  BadAtom (invalid Atom parameter)

Major opcode of failed request:  18 (X_ChangeProperty)

Atom id in failed request:  0x0

Serial number of failed request:  11

Current serial number in output stream:  12

--------------------------------------------------------------------

please help me

~Vaisakh N


Labels (2)
0 Kudos
1 Solution
768 Views
andre_silva
NXP Employee
NXP Employee
0 Kudos
2 Replies
768 Views
YixingKong
Senior Contributor IV

Vaisakh, please click Correct Answer if Andre's answer is good one.

Thanks,

Yixing

0 Kudos
769 Views
andre_silva
NXP Employee
NXP Employee
0 Kudos