Integrated Temperature sensor on sabrelite_imx6

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Integrated Temperature sensor on sabrelite_imx6

2,264件の閲覧回数
mohamad-ahmad
Contributor III

hello,

does someone there know how many thermal sensors are integrated on the sabrelite_imx6q?

To this moment in my exploration I find there only one sensor.

Thanks for help,

Mohamad

ラベル(2)
0 件の賞賛
返信
2 返答(返信)

1,967件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

also it may be useful to look at

AN5215 i.MX6 Temperature Sensor Module

http://cache.nxp.com/files/microcontrollers/doc/app_note/AN5215.pdf

~igor

1,967件の閲覧回数
gary_bisson
Senior Contributor III

Hi Mohamad,

There's one thermal sensor inside the i.MX6Q, the SabreLite board itself doesn't provide any more sensor than that.

For more information on this sensor, please read the i.MX6QD Reference Manual Chapter 62 (TEMPMON).

You can also have a look at the driver:

linux-imx6/imx_thermal.c at boundary-imx_3.14.52_1.1.0_ga · boundarydevices/linux-imx6 · GitHub

Hope this helps.

Regards,

Gary