Integrated Temperature sensor on sabrelite_imx6

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Integrated Temperature sensor on sabrelite_imx6

1,173 Views
mohamad-ahmad
Contributor III

hello,

does someone there know how many thermal sensors are integrated on the sabrelite_imx6q?

To this moment in my exploration I find there only one sensor.

Thanks for help,

Mohamad

Labels (2)
0 Kudos
Reply
2 Replies

876 Views
igorpadykov
NXP Employee
NXP Employee

also it may be useful to look at

AN5215 i.MX6 Temperature Sensor Module

http://cache.nxp.com/files/microcontrollers/doc/app_note/AN5215.pdf

~igor

876 Views
gary_bisson
Senior Contributor III

Hi Mohamad,

There's one thermal sensor inside the i.MX6Q, the SabreLite board itself doesn't provide any more sensor than that.

For more information on this sensor, please read the i.MX6QD Reference Manual Chapter 62 (TEMPMON).

You can also have a look at the driver:

linux-imx6/imx_thermal.c at boundary-imx_3.14.52_1.1.0_ga · boundarydevices/linux-imx6 · GitHub

Hope this helps.

Regards,

Gary