Integrated Temperature sensor on sabrelite_imx6

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Integrated Temperature sensor on sabrelite_imx6

2,324 次查看
mohamad-ahmad
Contributor III

hello,

does someone there know how many thermal sensors are integrated on the sabrelite_imx6q?

To this moment in my exploration I find there only one sensor.

Thanks for help,

Mohamad

标签 (2)
0 项奖励
回复
2 回复数

2,027 次查看
igorpadykov
NXP Employee
NXP Employee

also it may be useful to look at

AN5215 i.MX6 Temperature Sensor Module

http://cache.nxp.com/files/microcontrollers/doc/app_note/AN5215.pdf

~igor

2,027 次查看
gary_bisson
Senior Contributor III

Hi Mohamad,

There's one thermal sensor inside the i.MX6Q, the SabreLite board itself doesn't provide any more sensor than that.

For more information on this sensor, please read the i.MX6QD Reference Manual Chapter 62 (TEMPMON).

You can also have a look at the driver:

linux-imx6/imx_thermal.c at boundary-imx_3.14.52_1.1.0_ga · boundarydevices/linux-imx6 · GitHub

Hope this helps.

Regards,

Gary