Hi Istvan Bosznai,
First and just to make sure, I’m assuming that you are using the KITPFPGMEVME REV B (KITPFPGMEVME should have a sticker on the bottom with “REV B” on it), please correct me if I’m wrong.
An important notice is that you will not be able to work correctly with the GUI 4.0 until you have the KITPFPGMEVME connected to the target board, however, the programmer should be detected when connected.
Now, I would recommend you to download the latest revision of the KITPFGUI_4.1 (REV 4.1.0.6) from the following link and test with this revision of the GUI: http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=KITPFPGMEVME&fpsp=1&tab=Design_Tools_...
With this version of the GUI (4…), the NI-VISA software is no longer needed, so you should not have this issue anymore.
You can find the Use Guide for this version of the GUI on the following link: http://cache.freescale.com/files/analog/doc/user_guide/KTPFSWUG4.pdf
And additionally the KITPFPGMEVME Rev B Programmer User Guide in the following link: http://cache.freescale.com/files/analog/doc/user_guide/KTPFPGHWUG.pdf
Have a great day,
Jose Reyes
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------