Installing debian on imx6UL evk

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Installing debian on imx6UL evk

跳至解决方案
3,721 次查看
pratyushtomar
Contributor IV

I have already tried yocto on imx6UL evk successfully. Now I want to try installing console based debian on imx6UL evk. Is their any ready built debian image available for this or any method how to build and install debian linux on imx6UL evk?

标签 (2)
1 解答
2,273 次查看
Yuri
NXP Employee
NXP Employee

Hello,

    The following may be useful

Debian on the i.MX6 sabre sd platform in a few commands

Debian Jessie Rootfs

Debian Jessie on i.MX6

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

2 回复数
2,274 次查看
Yuri
NXP Employee
NXP Employee

Hello,

    The following may be useful

Debian on the i.MX6 sabre sd platform in a few commands

Debian Jessie Rootfs

Debian Jessie on i.MX6

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

2,273 次查看
cyriacdevasia
Contributor I

I found this site helpful. Followed the instructions (which are remarkably concise and clear) and have debian running on iMX6UL-EVK board.

MCIMX6UL-EVK - Linux on ARM - eewiki 

0 项奖励
回复