Installing Ubuntu using Mfgtools

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Installing Ubuntu using Mfgtools

1,653 Views
kovzone
Contributor I

Dear All,

I really new to this area. I've got complete files of Mfgtools with it's Ubuntu Trusty image (trusty.tgz). I run the mfgtools with serial download mode to install the ubuntu to eMMC, and it works fine. But after I restart the board (boot from eMMC), it's give me only blank screen (trough HDMI). Do you know why? Should I extract the trusty.tgz file under "Mfgtools-HOBBITQ-Ubuntu-1.0\Profiles\MX6Q Linux Update\OS Firmware\files"? 

Thank you,

Labels (2)
Tags (1)
0 Kudos
Reply
1 Reply

1,523 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Which board are you using? Have your u-boot success boot up, you need to set the kernel parameters in you u-boot.

0 Kudos
Reply