Installing Ubuntu using Mfgtools

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Installing Ubuntu using Mfgtools

1,684件の閲覧回数
kovzone
Contributor I

Dear All,

I really new to this area. I've got complete files of Mfgtools with it's Ubuntu Trusty image (trusty.tgz). I run the mfgtools with serial download mode to install the ubuntu to eMMC, and it works fine. But after I restart the board (boot from eMMC), it's give me only blank screen (trough HDMI). Do you know why? Should I extract the trusty.tgz file under "Mfgtools-HOBBITQ-Ubuntu-1.0\Profiles\MX6Q Linux Update\OS Firmware\files"? 

Thank you,

ラベル(2)
タグ(1)
0 件の賞賛
返信
1 返信

1,554件の閲覧回数
Rita_Wang
NXP TechSupport
NXP TechSupport

Which board are you using? Have your u-boot success boot up, you need to set the kernel parameters in you u-boot.

0 件の賞賛
返信